Technical FAQs

Ask a Question

What are the repair parts for a QO112L125GK, Series S1?

Only the parts listed below are considered field replaceable.
Cover - QOC16UF/S
Interior - QO112L125GI
Neutral Bonding gardware - 4028345850K
Main Lugs - QOL125
Cover mounting screw - 4020513002K (10 Pack)
Cover door hinge - 4028356450K (Kit contains parts to repair one hinge)
Cover latch and spring - 4020284450K
Main circuit breaker breaker and main lugs keps nut - 2342702001
Wiregator Inserts - 4055615301
Wiregator wireguard shields - 4055943550, QTY - 2.


CTA-ID : 2339
Was this helpful?
What can we do to improve the information ?