Technical FAQs

Ask a Question

What is the maximum ampere breaker that will fit into the MA1200S circuit breaker enclosure?

The maximum ampere breaker is 1200 ampere, types MAL, MHL, and MXL, but for DC only. The device is NOT marked for AC.

CTA-ID : 2034
Was this helpful?
What can we do to improve the information ?