Technical FAQs

Ask a Question

What is the color code for Type X relay cartridges?

The standard cartridge is black, the overlapping cartridges are red, the logic reed cartridges are grey, and master cartridges are blue. On all cartridges, the NO symbol is printed on a green background and the NC symbol is printed on a yellow background.


CTA-ID : 1719
Was this helpful?
What can we do to improve the information ?