Technical FAQs

Ask a Question

What is the replacement for a Q22225NRB circuit breaker enclosure for a Q2L circuit breaker?

Cross Reference

Product Line:
Circuit Breaker Enclosure

Cross Reference

The Q22225NRB was restricted to a 2-pole, 225A, Q2L circuit breaker. A Q23225NRB could be used to replace it for a breaker rated up to 225 ampere. If the Q2L breaker is a 200 ampere or less breaker, you could also consider a Q22200NRB enclosure.

CTA-ID : 1713
Was this helpful?
What can we do to improve the information ?