Technical FAQs

Ask a Question

What is the mounting dimension requirements for the XB4 or XB5 lines?

The hole size is 22mm or 7/8 inch diameter. Side to side mounting 30mm or 1.18`` center to center and from top to bottom 40mm or 1.57`` center to center.

CTA-ID : 1440
Was this helpful?
What can we do to improve the information ?