Technical FAQs

Ask a Question

31096-400-50 found in digest not on Q2C. This is supposed to be a 120V coil for the Size 5 starter but it doesn`t come up in Quote to Cash.

There`s a typo on page 13-118 of this digest. The prefix shown for Series B size 5 starters is wrong. It should be 31096-320-50.

CTA-ID : 1429
Was this helpful?
What can we do to improve the information ?