Technical FAQs

Ask a Question

What is the trip unit adjustment range on CK 800 amp breaker CKAEL36808LI and CM CMEF36200LI breaker?<br />STR DE SP UP UE

Per page 49 of 99 Pricing Guide the CK STRxxDE, SP and UP trip unit are adjustable from 0.8 to 1 times plug rating.
STRxxDE, SE and UE trip units are adjustable from .4 to 1.0 times the sensor rating. The CM ST206D trip rating is adjustable from .5 to 1.0 times sensor rating.


CTA-ID : 2334
Was this helpful?
What can we do to improve the information ?