Technical FAQs

Ask a Question

Received a neutral current transformer with the GFM250. Is the neutral current transformer needed to make the ground fault on the breaker work?

The neutral is needed if there is a load neutral. If you do not have a neutral you do not need the neutral current transformer. However, the system needs to be solidly grounded.

CTA-ID : 2019
Was this helpful?
What can we do to improve the information ?