Technical FAQs

Ask a Question

What are the differences between the XB2BS9445 and its replacement the XB4BS9445?

Issue:
What are the differences between the XB2BS9445 and its replacement the XB4BS9445?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
They use different mounting collars. The new XB4 line has be designed for easier installation. Its mounting collar only has one screw. It also uses snap on contact blocks.


CTA-ID : 803
Was this helpful?
What can we do to improve the information ?