Technical FAQs

Ask a Question

What are the horsepower ratings for the Class 8911 Type DPSO13 & DPSG13?

115 VAC 1 PH = 1 HP
230 VAC 1 PH = 2 HP
230 VAC 3 PH = 3 HP
460/575 VAC 3 PH = 5 HP


CTA-ID : 794
Was this helpful?
What can we do to improve the information ?