Technical FAQs

Ask a Question

What is the suffix number for a molded case circuit breaker with a 120v shunt trip and 1-N/O and 1-N/C auxiliary contact?

Suffix number 1380 (Three pole module breakers only, ie a 2 pole KAL is a in a 3 pole case).


CTA-ID : 787
Was this helpful?
What can we do to improve the information ?