Technical FAQs

Ask a Question

What is the length of the interior for a NQOD 150 A main breaker with 30 circuits?

39.88 inches. Dimensional information can be found in the Class 1630 NQOD circuit Breaker Panelboards, Catalog # 1630CT9701, at

CTA-ID : 407
Was this helpful?
What can we do to improve the information ?