Technical FAQs

Ask a Question

What is the recommended mounting height for panelboards?

NEC states that circuit breakers shall be installed so that the center of the grip of the operating handle of the circuit breaker when in its highest position will not be more than 6 ft 7 in. above the floor or working platform. NEC 380-8a.


CTA-ID : 405
Was this helpful?
What can we do to improve the information ?