Technical FAQs

Ask a Question

Is EZM116125 a single row of 6 sockets high or two rows of 3 sockets high?

It is a single row of 6 sockets high.


CTA-ID : 772
Was this helpful?
What can we do to improve the information ?