Technical FAQs

Ask a Question

When is the AD Module required?

It is required for accurate ammeter indications for loads less than 20% of the current sensor rating, for ``V`` (remote selected fault indication) option, and for ``T`` or ``W`` (ground fault) option for the lower settings (settings in the red zone).

CTA-ID : 478
Was this helpful?
What can we do to improve the information ?