Technical FAQs

Ask a Question

Need to know actual mounting hole spacing on the 82342.

The mounting holes are 12.75``W x 11.44``H, the holes are .32`` diameter. The mounting hole spacings are the same for 82352. This information is available on Approval Drawing #2165.

CTA-ID : 756
Was this helpful?
What can we do to improve the information ?