Technical FAQs

Ask a Question

How can I find the combination suffix for more than two devices installed on a circuit breaker?

In the class 601 Thermal-Magnetic/Magnetic Only Molded Case Circuit Breakers manual on page 79 is a matrix that can be used to obtain the combination suffix for two devices installed into circuit breakers. This matrix does not include all combinations.


CTA-ID : 469
Was this helpful?
What can we do to improve the information ?