Technical FAQs

Ask a Question

Which circuit breakers come with integral padlock attachments?

The P frame breaker and the QOB-VH two- and three-pole breakers. The QOB-VH padlock attachment is located between the poles, to the right of the handle. The P frame padlock attachment Is located underneath the end of the handle.

CTA-ID : 456
Was this helpful?
What can we do to improve the information ?