Technical FAQs

Ask a Question

Can the shroud on an I-Line circuit breaker be replaced or repaired?

No, it is an integral part of the circuit breaker and can only be installed at the factory at the time of manufacture.


CTA-ID : 453
Was this helpful?
What can we do to improve the information ?