Technical FAQs

Ask a Question

I need lugs to bring 4 - #3/0 wired into an MH36800 or MHL36800.

See Mechanical Lug page of Circuit Breaker section of the Digest.
Use AL1000MA for 4 - #1/0AWG to 350kcmil for copper or aluminum conductors. These lugs will fit MA(L), MH(L), ME(L), and MX(L) breakers 300A to 1200A.


CTA-ID : 744
Was this helpful?
What can we do to improve the information ?