Technical FAQs

Ask a Question

Can 1200 A lugs be installed in an 800A CK breaker?

Yes, two options are available with maximum wire sizes of (4) 500 MCM or (3) 600 MCM per phase.


CTA-ID : 444
Was this helpful?
What can we do to improve the information ?