Technical FAQs

Ask a Question

Can a double throw switch be provided with a key interlock?

Issue:
Availability of keyed interlocks on a double throw safety switch.

Product Line:
Heavy Duty Safety Switches

Environment:
Safety switches sold and supported in the USA.

Cause:
Availability and procedure to select a keyed interlock for a double throw safety swith.

Resolution:
Yes, keyed interlocks can be ordered as factory assembled only.  For ordering information, refer to the Digest Plus Product Selector, available on-line at www.squared.com.

  








CTA-ID : 306
Was this helpful?
What can we do to improve the information ?