Technical FAQs

Ask a Question

What are the rail and deadfront extensions required to mount an NQOD430L100 or NQOD430L100CU in an MH29 or MH29WP?

The following parts will be required per panel and can only be installed at the mains end:

(2) 80110-288-01 3`` rail extensions
(1) 80110-290-01 MLO cover deadfront extension
(4) 21590-17081 Rail extension screws

Revised 3/10/04

CTA-ID : 726
Was this helpful?
What can we do to improve the information ?