Technical FAQs

Ask a Question

What operating handle should be used with the Class 9422 Type RX1 circuit breaker operating mechanism?

Class 9422 Type A1 through A4 will work. However Class 9422 Type A1 or A2 is recommended due to leverage issues with the smaller Type A3 or A4 handle assemblies.


CTA-ID : 687
Was this helpful?
What can we do to improve the information ?