Technical FAQs

Ask a Question

Can a double throw safety switch be provided with a neutral assembly?

The 82000 and 92000 line of Double Throw safety switches do not have field installable neutral assemblies available. For factory installation of a neutral assembly, add suffix N to the catalog number. The DTU line, Series E design, are supplied with a factory installed neutral assembly as a standard feature. The DT and DTU line, Series F design, have neutral assemblies available for field installation.


CTA-ID : 297
Was this helpful?
What can we do to improve the information ?