Technical FAQs

Ask a Question

Will the KA36225 accept 1-2/0 cable per phase

Yes, the standard lug will accept (1) #4 AWG to 350 kcmil per phase, Cu or Al conductor.


CTA-ID : 701
Was this helpful?
What can we do to improve the information ?