Technical FAQs

Ask a Question

What electrical interlock kits are used with Heavy Duty safety switches?


Product Line:
HD SS Accessory


The Electrical Interlock Kit would vary, dependent upon the safety switch that it is to be used in. 
For current design safety switches, refer to the current Schneider Electric Digest, available on-line at
For obsolete designs, refer to the wiring diagram provided on the inside cover of the safety switch or contact 1-888-778-2733, Opt 1, Opt 1, Opt 4 with the switch catalog number and series number. 

CTA-ID : 377
Was this helpful?
What can we do to improve the information ?