Technical FAQs

Ask a Question

What is the distance from the cross bus of EZM to the bottom endwall?

This dimension is not needed in order to mount an EZM line-up. The crossbus of the EZM devices will line up correctly when the devices are mounted so that the mounting channels on each unit are lined up across the wall.

CTA-ID : 231
Was this helpful?
What can we do to improve the information ?