Technical FAQs

Ask a Question

What is the maximum number of spaces available in the Meter Mains and All-In-One CSED devices?

Issue:
Current product design

Product Line
Combination Service Entrance Devices

Environment:
Interior spaces

Cause:
Application

Resolution:
The maximum number of spaces will depend on the catalog number of the device and if the device is a Meter Main or an All-In-One. Refer to each catalog number in the Digest Plus Product Selector, available on-line at  www.squared.com


CTA-ID : 281
Was this helpful?
What can we do to improve the information ?