Technical FAQs

Ask a Question

Can MP or MPR Meter-Pak Meter Centers be supplied with a lever by-pass?

Lever by-pass options are available in a 2,3 and 4 position, Ringless only Meter-Pak. Catalog numbers begin with MPL... See Residential catalog page 40.

CTA-ID : 234
Was this helpful?
What can we do to improve the information ?