Technical FAQs

Ask a Question

Can I mount branch devices on both sides of an EZM line-up?

Yes. Branch devices can be mounted on both sides of the main device. In fact, the main device must be center mounted if its amperage rating is larger than the amperage rating of the cross bus of the branch devices.

CTA-ID : 229
Was this helpful?
What can we do to improve the information ?