Technical FAQs

Ask a Question

What is the diameter of the rod used on the ZCKY91 lever arm?

The straight rod is 3 mm or 0.12`` in diameter, while its coiled spring base is 8mm or 0.31 `` in diameter


CTA-ID : 681
Was this helpful?
What can we do to improve the information ?