Technical FAQs

Ask a Question

Are neutral assemblies available for not-fusible General Duty switches?

Neutral Assembly SN0610 is available for DU323 or DU323RB, Series F1 or F3. Neutral Assembly SN20A is available for DU324 or DU324RB, Series F1, or Neutral Assembly SN225KA for DU324 or DU324RB, Series E2 or E3. Neutral Assembly D600SN is available for DU326, Series E1 or E3. No other not-fusible General Duty switches will accept a neutral assembly.

CTA-ID : 217
Was this helpful?
What can we do to improve the information ?