Technical FAQs

Ask a Question

What ground block can be used with a 9080M46G?

There is no grounding block the same size as the 9080M46G. See the units in Digest 171 20-9 for the available 9080 Type M grounding terminals. Any of them can be used.


CTA-ID : 768
Was this helpful?
What can we do to improve the information ?