Technical FAQs

Ask a Question

What is the contact block with 2 normally closed contacts the same as the 9001KA3G.

There is no single block with 2 normally closed contacts. Use two 9001KA3G blocks.


CTA-ID : 667
Was this helpful?
What can we do to improve the information ?