Technical FAQs

Ask a Question

What is the meaning of Form X for the 9013 pressure switches?

Form X adds a two-way pressure release valve. This valve opens mechanically when the electrical contacts open, and may be used to bleed pressure from the head of a compressor to allow startup without load. May be field replaced, not field added.


CTA-ID : 277
Was this helpful?
What can we do to improve the information ?