Technical FAQs

Ask a Question

What is the maximum voltage applicable to General Duty safety switches?

Issue:
Application

Product Line:
GD SS

Cause:
Application

Resolution:
The General Duty Safety Switches are rated for use on a 240Vac maximum voltage system. The are not rated for use on dc voltage systems; refer to Heavy Duty Safety Switches for applications up to 600Vac; 600Vdc.


CTA-ID : 171
Was this helpful?
What can we do to improve the information ?