Technical FAQs

Ask a Question

What is the 240 volt light module with 1 normally open and 1 normally closed contacts to use with a ZA2BW31?<br />

ZA2BW0945 is a 240 volt transformer light module, 1 normally open and 1 normally closed contacts, and mounting collar.


CTA-ID : 643
Was this helpful?
What can we do to improve the information ?