Technical FAQs

Ask a Question

What is the part number for the cover only, for the XVBC indicating bank?

XVBC081 is cover only. It is also included with the base in a XVBC21.


CTA-ID : 646
Was this helpful?
What can we do to improve the information ?