Technical FAQs

Ask a Question

What is the housing rating for the 9012G?

NEMA 4, 4x and 13 Enclosure, or NEMA 7 and 9, depending on the part number selected.


CTA-ID : 210
Was this helpful?
What can we do to improve the information ?