Technical FAQs

Ask a Question

What is the housing material made of on the 9012 pressure switch and what paint is used?

NEMA 7 & 9 types: cast iron or cast aluminum Open Type and NEMA 1: back plate is steel and cover is plastic. All others are cast aluminum alloy, with baked enamel coating.

CTA-ID : 206
Was this helpful?
What can we do to improve the information ?