Technical FAQs

Ask a Question

How do I select the proper replacement contacts for an 8911DPSG33 starter?

These are the same contacts as used for the 8910DPA33, the 8911DPSG43 would use the 8910DPA43 contacts, and so on.


CTA-ID : 352
Was this helpful?
What can we do to improve the information ?