Technical FAQs

Ask a Question

What is the basic construction of a double throw switch?

A double throw switch has one OFF position and two ON positions. Internally, load wiring is connected to the center position. Line wiring is connected to one ON position from a Primary source and the other ON position from a Secondary source.

CTA-ID : 165
Was this helpful?
What can we do to improve the information ?