Technical FAQs

Ask a Question

Are the Meter Pak(MP) and EZM Metering, Meter Centers suitable for either indoor or outdoor applications?

Issue:
Product Design

Product Line:
Meter Pak and EZM Metering

Environment:
Enclosure Ratings

Cause:
Application

Resolution:
Yes. The Meter-Pak and EZM Metering equipment are outdoor NEMA 3R rated, but can also be used in indoor for NEMA 1 applications.
NOTE: The exception to the above, is the bussed corner section for EZM, and the busway tap EZM main devices.
 
Was this helpful?
What can we do to improve the information ?