Technical FAQs

Ask a Question

How many fuses are needed for the QMJ363T?

Product Design features

Product Line:
QMB Branch Switches

The QMJ363 is a 3pole TWIN switch, so it would be logical that a total of 6 - Class J, 600 Volt, 100 amp max, Fuses would be required. One fuse PER Pole for each 3pole switch.

CTA-ID : 919
Was this helpful?
What can we do to improve the information ?