Technical FAQs

Ask a Question

What is the ground fault module / relay to use with an FAL type breaker?

The ground fault module is GFM100FA. In conjuction with the module, the circuit breaker must have a ``G`` suffix, indicating a ``Ground-fault shunt trip``


CTA-ID : 915
Was this helpful?
What can we do to improve the information ?