Technical FAQs

Ask a Question

What is the maximum voltage applicable to Heavy Duty switches?

Heavy Duty switches are available for use on systems up to 600 Vac and 600 Vdc.


CTA-ID : 122
Was this helpful?
What can we do to improve the information ?