Technical FAQs

Ask a Question

Can single-phase branch devices be used with 3-phase main EZ Meter-Pak devices?

Yes. There are some branch devices that are 3-phase In/Single phase Out, which would be used in this application. Refer to the Digest Plus Selector at www.squared.com for branch selection.


CTA-ID : 109
Was this helpful?
What can we do to improve the information ?