Technical FAQs

Ask a Question

Can an EZ Meter-Pak Main Disconnect or Terminal Box be located anywhere in the metering lineup, with relation to the branch devices?

There are some restrictions. A 1000 Ampere or 1200 Ampere Main Disconnect or Terminal Box must be center mounted when used with branch devices that have 800 Ampere cross bussing. A 1600 Ampere Main Disconnect or Terminal Box must always be center mounted.


CTA-ID : 107
Was this helpful?
What can we do to improve the information ?