Technical FAQs

Ask a Question

Can an EZ Meter-Pak branch device that normally accepts 125 Ampere branch breakers be converted to accept 200 Ampere branch breakers?

No. Branch devices are designed to accept branch breakers rated at a maximum of 125 Ampere, 200 Ampere or 400 Ampere. A device designed to accept a smaller frame of breaker cannot be modified to accept larger frame branch breakers.

CTA-ID : 102
Was this helpful?
What can we do to improve the information ?